Instructions
Does FLIR offer an SDK to control and get video stream from the FLIR IR cameras?
Learn moreTechnical Guidance
Can I control the A320 or A325 (A320G) camera using serial communication, RS-232?
Learn moreSystem Requirements
Which lens alternatives can I get with A310, A320, A315 and A325 (A320G)?
Read the StoryTechnical Guidance
Are cameras such as the X6900SC / X6800SC / X8500SC fully GeniCam compliantl?Are there any restrictions (maximum framerate, superframing, preset sequencing) in doing so, or is it full control?
Learn moreInstructions
I see that there are two firmware versions for the A3xx cameras. Which one should I choose?
Read the Story