Troubleshoot Breakdowns Before They Happen

Electrical / Mechanical Inspections

A solid predictive maintenance program can make the difference between meeting or missing production deadlines. So many companies rely on FLIR thermal imaging and Test & Measurement tools to survey and troubleshoot mechanical equipment and electrical systems. These tools allow technicians to inspect energized equipment safely—even at peak operation. Along with troubleshooting, thermal imaging cameras and non-contact measurement tools can also help optimize the production process and monitor quality control.

FLIR saves us from electrical hot spots failing, that would cause lots of down time. We repair spots identified by the IR test and repair before failure.

Electrician, Large Enterprise Industrial Manufacturing Company

Source: TechValidate. TVID: F7A-DDA-1C4

Thermal images for Electrical and Mechanical applicationsFind it, Diagnose it, Fix it

See Initial Signs of Failure

A thermal imaging camera allows you to quickly scan large areas, looking for hot spots on machinery or electrical systems that could indicate a potential problem.

Diagnose the Source of the Problem

With built-in meter features such as LoZ mode, and in-camera temperature analysis options, FLIR's range of professional tools helps you quickly diagnose problems and get to the job of fixing them.

Demonstrate that it's Repaired

Thermal images provide visual proof a fault existed and was properly repaired. Including these shots and measurement data in your reports will help to document your work and increase customer confidence.

 

Recommended Solutions for
Electrical/Mechanical Applications

FLIR CM275

IGM™ Clamp Meter with Datalogging (Wireless)

FLIR T1010

HD Thermal Imaging Camera

FLIR E86

Advanced Thermal Imaging Camera

product category

Target Problems Quickly with IGM™

Finding the source of an electrical failure can turn into a guessing game if you’re using a thermocouple or spot IR gun. FLIR IGM products combine thermal imaging with clamp meters or digital multimeters, so you can find hot spots visually and then quickly start on repairs.

FLIR DM285

Industrial Imaging Multimeter with IGM™

 


 

Discover More
Choosing a Camera

5 Tools an Electrical Contractor Can't Live Without

Learn more
Fundamentals

How Far Can You Measure with a Thermal Camera?

Learn more
Choosing a Camera

What Is the Right Handheld Thermal Camera for You?

Learn more
Tech Note

You Can’t Afford to Forget ‘FORD’ – 3 Things to Remember During an IR Inspection

Read the Story